Menu

NYSE:

ROK

218.96
Change:
-3.24 -1.46%
Volume: 774,124
09/18/2020

Featured Presentation

November 20, 2019 Annual Investor Conference
View this Presentation (PDF 8.10 MB)

NYSE:ROK

Rockwell Automation Saves Costs, Simplifies Sizing with New Servo System

November 14, 2019

Allen-Bradley Kinetix 5100 servo drive can run without a controller to meet a range of performance needs

MILWAUKEE-- The growing consumer desire for more product variety and packaging sizes is creating a need for smaller, more flexible machines. To provide a more cost-effective option for OEMs building smaller machines, Rockwell Automation is introducing a new Kinetix 5100 servo drive, Kinetix TLP motor and cable that can function as a system without a controller.

The new Allen-Bradley Allen-Bradley Kinetix 5100 servo drive has multiple control modes available to support a wider range of high-speed, low-power motion control applications. The drive can be used with a Micro800 controller, a Logix controller or even by itself, allowing OEMs to choose how the product best functions in their applications.

“The Kinetix 5100 servo system works especially well for small- to mid-sized packaging machines that need cost-effective servo control,” said Simon Wong, product manager, Rockwell Automation. “Bundling the drive, motor and cable together creates more competitive system pricing. And the ability for OEMs to select the products based on a machine’s power ratings can save time and effort – and help them get to market faster. This approach and product portfolio positions Rockwell Automation to accelerate our growth in China and emerging markets.”

The Kinetix 5100 servo system can also help OEMs make customers more productive. With the explosion of SKUs, manufacturers are faced with multiple changeovers, which are often a manual process. Using the Kinetix 5100 servo drive, OEMs can create a motorized, or automated, system that can help speed up changeovers.

Additionally, with built-in safe torque off, users can remove motor torque without removing power from an entire machine, allowing a machine to restart faster after it has reached a safe state. Dual-port EtherNet/IP also supports device-level ring topologies.

The Kinetix 5100 servo drive provides an easy migration option for users of the Allen-Bradley Ultra 3000 digital servo drive. That system will soon be phased out in favor of the Kinetix 5100 servo drive.

About Rockwell Automation

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more productive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 23,000 problem solvers dedicated to our customers in more than 100 countries. To learn more about how we are bringing The Connected Enterprise to life across industrial enterprises, visit www.rockwellautomation.com.

Media Contacts:
Stephanie Winterhalter
Rockwell Automation
414.795.6506
sawinterhalter@ra.rockwell.com

Ike Umunnah
Rockwell Automation
414.382.5679
itumuna@ra.rockwell.com

Allen-Bradley, Kinetix and Micro800 are trademarks of Rockwell Automation Inc.
EtherNet/IP is a trademark of ODVA.


Top