Menu

NYSE:

ROK

177.39
Change:
+1.95 +1.11%
Volume: 702,588
02/15/2019

NYSE:ROK

Software Reduces Design Time for Standalone Machines

July 12, 2018

Latest release of Connected Components Workbench software creates a more familiar and efficient design environment

MILWAUKEE — Machine builders can now get standalone machines to market faster using a newly updated design and configuration software. The latest release of the Connected Components Workbench software from Rockwell Automation will be more familiar to Logix users and includes new features to help reduce programming time. It provides controller programming, device configuration and human-machine interface editing for Rockwell Automation hardware.

A new instruction toolbar organizes programming elements into tabs. This allows designers to easily search, drag and drop instructions into the ladder logic editor. For designers who prefer the keyboard, ladder logic can be quickly entered in ASCII text. Designers also can now switch instruction names from the default IEC theme to a Logix theme. This can help them be more efficient by programming machines using their preferred terminology.

“Designers who use the RSLogix 500 or Studio 5000 Logix Designer software will now have a more familiar design environment in the Connected Components Workbench software due to a more seamless and standardized design experience,” said Thomas Sugimoto, product marketing manager, Rockwell Automation. “It also reduces training and simplifies maintenance for technicians by providing a consistent monitoring and debugging environment across a wider range of machines.”

Designers can now copy and paste code from the Connected Components Workbench software to the RSLogix 500 or Studio 5000 software and vice versa. This ability to reuse code can help designers modernize their small standalone machines from Allen-Bradley MicroLogix controllers to Micro800 controllers. It also can help them standardize larger machines that use Allen-Bradley CompactLogix controllers.

The Connected Components Workbench software supports all Micro800 controllers, including the new Micro870 programmable logic controller (PLC). This controller can be used in place of multiple micro PLCs in large standalone smart machines or systems. The software also supports the PanelView 800 graphic terminals, PowerFlex drives, SMC soft starters, Kinetix component servo drives and various safety devices such as the Guardmaster 440C-CR30 safety relay and GuardShield 450L light curtain.

About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.

Media Contacts
Patti Vivolo
Rockwell Automation
pvivolo@ra.rockwell.com

Keegan Leddy
Padilla
612.455.1941
keegan.leddy@padillaco.com

Allen-Bradley, Connected Components Workbench, CompactLogix, Guardmaster, GuardShield, Kinetix, Logix, Micro800, Micro870, MicroLogix, PanelView, PowerFlex, RSLogix 500, SMC and Studio 5000 are trademarks of Rockwell Automation Inc.


Top