Menu

NYSE:

ROK

194.07
Change:
+2.62 +1.37%
Volume: 940,636
09/18/2018

Featured Presentation

August 10, 2018 Rockwell Automation: Overview August 2018
View this Presentation (PDF 7.64 MB)

NYSE:ROK

Safer, Smarter Operations with the New GuardLink Safety System

April 12, 2018

Connected technology reduces maintenance and increases reliability

MILWAUKEE, April 12, 2017 — Rockwell Automation introduces the Allen-Bradley Guardmaster GuardLink safety system, a new safety-based communications protocol that helps operators reduce and improve machine diagnostics and downtime while increasing productivity.

Traditionally, safety devices are wired to separate safety inputs, which requires significantly more wiring and introduces more potential fault points. When wired in this series connection, customers lose the ability to distinguish information from each device. With GuardLink, safety devices are easily connected in series while providing access to individual device diagnostics. This system provides safety, diagnostics, remote reset and lock command over a single four conductor cable with up to 32 devices per link. In addition, customers can greatly reduce installation cost, with up to 38 percent reduction in wiring, when using GuardLink.

The GuardLink technology seamlessly integrates with Allen-Bradley Guardmaster safety relays and components, allowing users to access status information throughout their entire safety system. The connection of safety devices with smart taps enabled by GuardLink technology and standard cabling to a Guardmaster safety relay allows greater visibility into the system, down to individual guard doors and E-stops.

“When an e-stop or interlock switch is operated, the individual safety signal is sent to the Guardmaster safety relays,” said Thomas Helpenstein, safety product manager, Rockwell Automation. “That information is then communicated seamlessly across The Connected Enterprise via the Guardmaster network interface, making it easier and faster to diagnose and repair problems when compared to traditional wired systems.”

The GuardLink safety system fully integrates with the Logix platform with predetermined tag names in the Rockwell Software Studio 5000 application. Its simplified design and reduction in wires allows for simple plug-and-play installation.

About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.

Media Contacts
Todd Bissell
Rockwell Automation
978.446.3284
tmbissel@ra.rockwell.com

Dana Bossen
Padilla
612.455.1751
dana.bossen@padillaco.com

Allen-Bradley, GuardLink, Guardmaster, LISTEN. THINK. SOLVE., Rockwell Software and Studio 5000 are trademarks of Rockwell Automation Inc.
EtherNet/IP is a trademark of ODVA Inc.


Top