Menu

NYSE:

ROK

319.88
Change:
+3.74 +1.18%
Volume: 97,743
10/20/2021

NYSE:ROK

Rockwell Automation Joins Industry Effort on OPC UA Time-Sensitive Networking

April 24, 2018

Industry group is collaborating to address real-time device-to-device and device-to-cloud applications

MILWAUKEE, April 24, 2018 — Rockwell Automation is joining industry leaders ABB, Belden, Bosch Rexroth, B&R, Cisco, Hilscher, KUKA, National Instruments, Parker Hannifin, Phoenix Contact, Pilz, Schneider Electric, TTTech and WAGO (collectively known as Shapers) to create a communication solution for real-time and sensor-to-cloud applications in industrial operations. The solution will be based on the OPC UA protocol, which allows easy and secure sharing of information across different vendor technologies and the time-sensitive networking (TSN) suite of standards, which helps improve latency and robustness in converged industrial networks.

“Connecting technologies across an industrial organization while maintaining multivendor interoperability requires a harmonized, interoperable solution that uses consistent information models, communication and application behavior (together known as application profiles),” said Paul Brooks, business development manager, Rockwell Automation.

“That’s what this group of automation leaders are combining their expertise to create. Our solution will give manufacturing and industrial organizations best-of-breed I/O device control, motion and safety application profiles,” said Sebastian Sachse, B&R Industrial Automation.

To ensure the emerging OPC UA TSN solution supports interoperability of different vendor technologies on the same network, the companies are engaging with industry consortia such as Avnu, IEEE, IIC, LNI 4.0 and OPC Foundation. The companies are also planning an announcement in the coming months on how to achieve unified application profiles, which is the last hurdle to device harmonization. They aim to provide one-stop-shop certification of the overall solution up to the device-profile level.

The companies have already published whitepapers on OPC UA TSN technology, such as an IIC whitepaper on converged traffic types. They have also made significant contributions to the recently released PubSub extension of OPC UA, and plan to set up a collaboration between the IIC and LNI testbeds.

About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.

Media Contacts
Paul Brooks
Rockwell Automation
pbrooks@ra.rockwell.com  

Sebastian Sachse
B&R
sebastian.sachse@br-automation.com  

LISTEN. THINK. SOLVE. Is a trademark of Rockwell Automation Inc.


Top