Menu

NYSE:

ROK

227.39
Change:
+4.90 +2.2%
Volume: 1,043,873
06/05/2020

NYSE:ROK

New Micro PLC Can Reduce Complexity of Large Standalone Machines

March 29, 2018

Allen-Bradley Micro870 PLC, new flagship of Micro800 family, can be used in place of multiple micro PLCs

MILWAUKEE, March 29, 2018 — Machine designers can use a new micro programmable logic controller (PLC) to help optimize the control architecture in large standalone machines or systems. The new Allen-Bradley Micro870 PLC can support smart micro applications that require up to 304 I/O points, 280 KB of memory and 20,000 program instructions.

“Designers today use several PLC sizes for their automation projects” said Yeow Keng Teh, product manager, micro controllers, Rockwell Automation. “This approach requires inventory management of the different PLC sizes and maintenance of different programs. Now designers can use the Micro870 PLC to scale their controller to their application needs. This helps simplify inventory management, especially for those designing multiple machine types.”

The Micro870 PLC uses a flexible design concept that provides designers up to three plug-ins and eight expansion I/O modules. This capability allows them to easily customize or expand the controller to meet each machine type’s unique requirements.

The controller’s 280 KB memory capacity supports modular programming and the use of user-defined function blocks to help reduce design time. Additionally, machine builders can use this memory capacity to maintain a single program for all machine models that use the Micro870 PLC.

The controller communicates via EtherNet/IP and includes multiple embedded communications options, including a USB programming port, a non-isolated serial port and an Ethernet port. It can also support up to two axes of motion.

The new Connected Components Workbench software version 11 provides a single design environment for programming the Micro870 PLC. The software can also be used to configure Allen-Bradley PanelView 800 graphic terminals, PowerFlex AC drives, Kinetix component servo drives, electronic overload relays, light curtains and configurable safety relays. This feature can save engineers time and costs compared with using another programming tool for each device in a system.

A new conversion tool in version 11 makes it easier for MicroLogix customers to upgrade to the Micro800 controller family. In addition, version 11 allows Encompass members of the PartnerNetwork program to help ease configuration of complementary third-party products via graphical configuration profiles. These profiles support the Micro800 plug-ins as well as expansion I/O to help make the configuration process faster and more accurate.

About the Rockwell Automation PartnerNetwork Program
The Rockwell Automation PartnerNetwork program offers global manufacturers access to a collaborative network of companies mutually focused on developing, implementing and supporting best-in-breed solutions to achieve plant-wide optimization, improve machine performance and meet sustainability objectives.

About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.

Media Contacts
Patti Vivolo
Rockwell Automation
pvivolo@ra.rockwell.com

Keegan Leddy
Padilla
612.455.1941
keegan.leddy@padillaco.com

Allen-Bradley, Connected Components Workbench, Encompass, Kinetix, LISTEN. THINK. SOLVE., Micro800, Micro870, MicroLogix, PanelView, PartnerNetwork and PowerFlex and are trademarks of Rockwell Automation Inc.
EtherNet/IP is a trademark of ODVA Inc.


Top