Menu

NYSE:

ROK

159.95
Change:
+0.80 +0.5%
Volume: 1,077,471
07/19/2019

NYSE:ROK

Advanced Light Curtain System Improves Flexibility and Safety

August 23, 2018

Rockwell Automation GuardShield light curtains bring innovative transceiver technology to safeguard perimeter of robotic work cells and other hazardous equipment

MILWAUKEE — The rise of robots has ushered in an increased demand for light curtains that provide a safe work environment between the robotic work cells and the rest of the plant. The Allen-Bradley GuardShield 450L safety light curtain system from Rockwell Automation is a flexible, cost-effective solution that enhances safety while improving productivity through innovative transceiver technology.

“Users will see significant advantages throughout the lifecycle of the new light curtain system, but especially during installation and operation,” said Manfred Stein, global product manager, Safety Light Curtains, Rockwell Automation.

The Integrated Laser Alignment System (ILAS) of the new GuardShield 450L-E reduces installation time by providing multiple visible laser points that optimize setup with a simple touch of the ILAS symbol on the front window of the stick. Plus, the compact design and full-length protective field make it easy to integrate a GuardShield 450L-E system in hand and finger protection applications from 150 mm (5.9 inches) up to 1950 mm (76.7 inches) in increments of 150 mm (0.5 foot).

After start-up, users can leverage advanced features and functionality, including cascading, built-in muting and blanking, to enhance flexibility while maintaining the highest level of safety.

The advanced muting and blanking functions of the GuardShield 450L-E light curtain are easily set up through DIP switches located on the dedicated plug-in modules. Common muting set ups like 4-sensor or 2-sensor with L- and T-configuration and override function can be selected as well as reduced resolution or teach in fixed blanking. A cascading plug-in can also be installed for series connection of additional GuardShield 450L Safety Light Curtain systems, enabling multi-sided machine guarding.
All these special functions combined with the inherent flexibility of the GuardShield 450L transceiver design help to simplify engineering logistics and minimize the stock required to address the full range of applications.

About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.

Media Contacts
Todd Bissell
Rockwell Automation
978.446.3284
tmbissel@ra.rockwell.com

Heidi Wight
Padilla
612.455.1795
heidi.wight@padillaco.com

Allen-Bradley and GuardShield are trademarks of Rockwell Automation Inc.


Top