Menu

NYSE:

ROK

167.30
Change:
+5.29 +3.27%
Volume:
04/25/2018

Featured Presentation

November 10, 2016 Conference: Rockwell Automation Investor Meeting
View this Presentation (PDF 25.67 MB)

NYSE:ROK

Latest Release of FactoryTalk Batch Software Introduces Modern Approaches for Batch Applications

November 07, 2016
Modern batch software from Rockwell Automation now improves batch responsiveness, scalability and productivity, and supports mobile devices

ATLANTA — Industrial producers with batch applications can now create more flexible, reliable and productive operations with the latest release of FactoryTalk Batch software from Rockwell Automation. The modern software enhances scalability and responsive control of distributed, skid-level phases with the integrity of plant-level coordination, while delivering an improved, reliable user experience with built-in mobility.

“Rather than trying to force-fit applications into rigid batch control systems, producers can now customize a modern batch system to their application’s needs,” said Dan UpDyke, product manager, Rockwell Automation. “These enhancements give batch producers greater flexibility when designing, operating and expanding batch systems. They also enable producers to use mobile devices for a more intuitive experience and improved workflows.”  

Integration with the SequenceManager solution from Rockwell Automation enables batch sequencing to occur at either the controller or server level. This allows machine builders to develop and deliver fully tested skids that end users can integrate into their batch process with minimal validation and commissioning effort. It also minimizes the rework required when manufacturers with small, controller-based batch systems expand to larger, server-based batch systems.

New mobile support can help create intuitive workflows, reduce procedural steps and increase collaboration. With mobile devices, workers no longer need to be bound to control rooms and fixed terminals. Instead, they can access real-time information, interact with processes and secure approvals from anywhere in a plant. A modern web interface also helps reduce the number of clicks required to access information.

News Release Asset
Image available upon request or here at box.com.

About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries. 

Media Contacts
Andrea Huter
Rockwell Automation
440.646.4195
ahuter@ra.rockwell.com

Molly O’Mara
PadillaCRT
612.455.1918
molly.omara@padillacrt.com


FactoryTalk and SequenceManager are trademarks of Rockwell Automation Inc.

Thumb Date Download
January 11, 2016 Quarterly Reports
January 10, 2016 News
January 9, 2016 SEC Filings

Top